{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I troubleshoot Supply Mains UnderVoltage faults on the Atlivar Process drives?
Issue:
Drive is tripping on Supply Mains UnderV (USF) fault code.

Product line:
Altivar Process, ATV630, ATV930, Altivar 600, Altivar 900

Environment:
all

Cause:
Supply voltage drops below trip level setting or transient drop in voltage.

Resolution:
Measure the line voltage with a meter.  Confirm the voltage reading matches on the Drive under the Main Menu > Display > Drive Parameters > Mains Voltage.

Check the settings for Undervoltage.  Go to Complete Settings > Error/Warning Handling > Undervoltage handling.
Mains Voltage (URES) should match the measured and monitored line voltage.  For example, if using a 240V drive and the supply voltage is only 208V then change Mains Voltage to 200 VAC.  If using a 480V drive and your supply voltage is 450-470V, then change the Mains Voltage to 460V.

UnderVolt Timeout (UST) - factory setting is 0.2 seconds.  Try increasing this to ride through a momentary voltage sag.

Schneider Electric Global