Search FAQs
What is the part number for the Profibus Fieldbus Option Module for the Altivar Process Drive?
Issue:
Part number of Profibus Fieldbus Option Module for the Altivar Process Drive.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
N/A
Resolution:
VW3A3607 - PROFIBUS DP Module for Altivar Process Drive with a sub-D 9 female connector
Part number of Profibus Fieldbus Option Module for the Altivar Process Drive.
Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)
Environment:
All serial numbers for Altivar Process Drive
Cause:
N/A
Resolution:
VW3A3607 - PROFIBUS DP Module for Altivar Process Drive with a sub-D 9 female connector
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: