Search FAQs
What do the different colors mean on the LED indicator for the Thermal Monitoring solution installed in the Model 6 Motor Control Center
An external single LED status indicator is provided on the unit disconnect mechanism for displaying thermal status conditions.
Solid Green - OK No Alarms No Color / Black - Not Operating / Loss of Power to Device
Solid Yellow - Phase Temperature Imbalance Flashing Yellow - Line / Load Delta Thermal
Flashing Red - High Temperature Solid Red - Sensor Failure Signal Loss
Temperature Alarms are configurable by dip switches.
The Thermal Monitoring solution includes Modbus RS485 serial communications capability. iMCC Network solutions with this feature are available under special order configurations.
For detailed installation and setup information reference the Exertherm instruction bulletin
For pricing and lead time information contact the Technical Assistance Group at the Seneca, SC manufacturing location.
Solid Green - OK No Alarms No Color / Black - Not Operating / Loss of Power to Device
Solid Yellow - Phase Temperature Imbalance Flashing Yellow - Line / Load Delta Thermal
Flashing Red - High Temperature Solid Red - Sensor Failure Signal Loss
Temperature Alarms are configurable by dip switches.
The Thermal Monitoring solution includes Modbus RS485 serial communications capability. iMCC Network solutions with this feature are available under special order configurations.
For detailed installation and setup information reference the Exertherm instruction bulletin
For pricing and lead time information contact the Technical Assistance Group at the Seneca, SC manufacturing location.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: