Search FAQs
Does the PM8000 support BACnet protocol?
Product Line:
PM8000
Environment:
BACnet
Resolution:
The PM8000 meters do not support BACnet protocol
Please follow this link to view what protocols are supported by the PM8000: Protocols, ports and connections
Notes:
The meter’s fundamental protocol and architecture is ION. You can integrate the meter into various industry-standard networks. Data that the meter measures can be made available to other devices using Modbus, DNP 3.0 and SNMP, as well as the MV-90 translation system. You can configure the meter to import data from other devices on these networks. The meter supports the IEC 61850 protocol and COMTRADE waveform data format. The meter also supports IPv6, DPWS and RSTP Ethernet protocols.