{}

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How to setup a ramp switching functionality on an ATV320 drive?
Issue:
Setting up ramp switching functionality on an ATV320 drive.

Product Line:
Altivar 320

Environment:
All

Cause:
Customer wanted a second deceleration with the drive.

Resolution:
This functionality allows activation of two different acceleration and deceleration rates based on a logic input or a frequency threshold.
In the SEt menu, parameters ACC and dEC are the first set of rates.

The ramp switching is programmable under ConF, FULL, FUn-, rPt-.

Parameter rPS is a ramp switching assignment for a logic input (LI1 thru LI6) or integrated communications.
Parameters AC2 (Acceleration 2) and DE2 (Deceleration 2) are the second set of rates.  The ATV320 uses ACC/dEC until the rPS assigned input goes active, at which point it uses AC2/dE2. Deactivating the input goes back to ACC/dEC rates.

Parameter Frt is a ramp 2 threshold activated when assigned a value other than 0Hz.  The ATV320 will use ACC/dEC when the output frequency is below Frt, but switch to AC2/dE2 when the output frequency is above Frt.

Note that if rPS is assigned and is at a logic state active, it will override the Ramp 2 Threshold setting (Frt) and the ATV320 will use AC2/dE2, regardless of the motor speed.

 

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.