{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Is the MCS025 Sync-Check module compatible with the SEPAM 40 or 20 series?

Issue
Need to be able to check voltage from another source using the Sepam relay.

Product Line
Sepam 20
Sepam 40
Sepam 80

Environment
Digital relays

Resolution
The MCS025 Sync-Check module only works for the Sepam 80 Series.  It is not compatible with the Sepam 40 or 20 series.  For more information on the MCS025 module, please refer to FA221262.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: