{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Is it possible to change the application type of Sepam 20, 40, 60 and 80. For example application type S80 to application type T87.

It is not possible to change the application type of the Sepam by the process of firmware upgrade change. The firmware upgrade does not affect at all the application type of the Sepam.

For Sepam 20 and 40, if the application type is not the desired one, depending on the country, most of the time the customer will need to purchase a new Sepam 20 or 40 with the correct application type.

For Sepam 60 and 80, the customer just need to purchase a new cartridge with the correct application type.

Please contact your local Schneider Electric representative to help with this issue. Depending on different circumstances, different actions will be done.

Schneider Electric Global

Explore more
Range:
AVEVA™ Plant SCADA
Explore more
Range:
AVEVA™ Plant SCADA
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.