{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What would cause a EPF2 fault using Profinet's telegram 1 and I/O profile on the ATV630 and ATV930 drives?
Issue:
EPF2 fault causes using Profinet and I/O profile on the ATV630 and ATV930 drives.

Product Line:
ATV630, ATV930

Environment:
All

Cause:
IO Profile and Telegram 1 are not compatible.

Resolution:
Profinet telegram 1 is not supported with IO Profile.  It is suggested that they use telegram 100 which does support IO Profile.

Schneider Electric Global