Search FAQs
Does the PSO PM5000S1 driver support DebugCategory and DebugLevel parameters?
Issue
Power SCADA Operation does not appear to support citect.ini parameters for DebugCategory and DebugLevel, making it impossible to activate verbose debugging at the driver level.
Product Line
Power SCADA Operation 8.2
PowerSCADA Expert 8.1
PowerSCADA Expert 8.0 SR1
PowerSCADA Expert 8.0
Environment
Power SCADA Citect.ini
Cause
The PM5000S1 driver is a legacy driver supporting older versions of PM5000 firmware and it inherits driver parameters from the parent driver (PM5000S).
Resolution
Instead of trying to add driver parameters in the citect.ini file for the PM5000S1, simply add them for the PM5000S driver family and both of the PM5000 drivers will log as configured.
Power SCADA Operation does not appear to support citect.ini parameters for DebugCategory and DebugLevel, making it impossible to activate verbose debugging at the driver level.
Product Line
Power SCADA Operation 8.2
PowerSCADA Expert 8.1
PowerSCADA Expert 8.0 SR1
PowerSCADA Expert 8.0
Environment
Power SCADA Citect.ini
Cause
The PM5000S1 driver is a legacy driver supporting older versions of PM5000 firmware and it inherits driver parameters from the parent driver (PM5000S).
Resolution
Instead of trying to add driver parameters in the citect.ini file for the PM5000S1, simply add them for the PM5000S driver family and both of the PM5000 drivers will log as configured.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: