{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

What are the specs for the fiber optic communication in the ION 8650 meter

Issue
Want to know the specification of fiber optic communication with the ION8650 meter

Product Line
ION8650

Environment
Fiber optic communication

Resolution
The part used for fiber optic communication is AFBR-5803AQZ from Broadcom Link to site.
Connector TypeSC
Data Rate125 MBd
EmitterLED
Fiber TypeMultimode Glass
Maximum Distance (m)2000
Nominal Optical Wavelength (nm)1300

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: