{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Which types and sizes of wires can be connected to the PRA90047 terminal?
In the PRA90047 it is possible to mount the following wires:
- from 0.5mm2 to 4mm2 - solid, flexible or flexible with ferrule.
- from 0.5mm2 to 6mm2 - solid or flexible (without ferrule).

Schneider Electric Global