Search FAQs
Does the HMIG3U support Dialog Table in Vijeo Designer?
Issue:
Checking compatibility of an old project when migrating to HMIG3U. Does the HMIG3U also support the dialog table feature?
Product Line:
Magelis, HMIG3U, Vijeo Designer
Resolution:
Yes, the HMIG3U supports the dialog table feature in Vijeo Designer when the appropriate protocol is used. For example, Modbus TCP/IP.
Note that protocols that use Tag names as device addresses do not support the Dialog Table. For example, Somachine or Pac Drive Ethernet.
Checking compatibility of an old project when migrating to HMIG3U. Does the HMIG3U also support the dialog table feature?
Product Line:
Magelis, HMIG3U, Vijeo Designer
Resolution:
Yes, the HMIG3U supports the dialog table feature in Vijeo Designer when the appropriate protocol is used. For example, Modbus TCP/IP.
Note that protocols that use Tag names as device addresses do not support the Dialog Table. For example, Somachine or Pac Drive Ethernet.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: