Search FAQs
How do I connect the main 3 phase power leads on an ATV212HU15N4? The terminal interface board is blocking access to the L2 and L3 terminal screws.
Issue:
How do I connect the main 3 phase power leads on an ATV212HU15N4? The terminal interface board is blocking access to the L2 and L3 terminal screws.
Product Line:
Altivar Machines, Altivar 212
Environment:
Frame size 1 ATV212 series drives: ATV212H: 075M3X,U15M3X, U22M3X, 075N4, U15N4, U22N4 U30M3X, U40M3X U30N4, U40N4, U55N4
Cause:
Terminal interface card blocks access to the L2 and L3 terminal screws.
Resolution:
Remove the terminal interface card first. There is a single #2 phillips screw in the center of the terminal interface card. It holds a plastic retainer strap in place. Remove the screw and fold the retainer strap to the right. Pull straight down on the terminal interface card to remove it, it should be easy to remove. Install your main power leads on L1, L2, L3 then reinstall the terminal interface card.
How do I connect the main 3 phase power leads on an ATV212HU15N4? The terminal interface board is blocking access to the L2 and L3 terminal screws.
Product Line:
Altivar Machines, Altivar 212
Environment:
Frame size 1 ATV212 series drives: ATV212H: 075M3X,U15M3X, U22M3X, 075N4, U15N4, U22N4 U30M3X, U40M3X U30N4, U40N4, U55N4
Cause:
Terminal interface card blocks access to the L2 and L3 terminal screws.
Resolution:
Remove the terminal interface card first. There is a single #2 phillips screw in the center of the terminal interface card. It holds a plastic retainer strap in place. Remove the screw and fold the retainer strap to the right. Pull straight down on the terminal interface card to remove it, it should be easy to remove. Install your main power leads on L1, L2, L3 then reinstall the terminal interface card.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: