{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to connect to the Masterpact MTZ via NFC [Video]

Article available in these languages: French, Dutch

Question:
How to connect to the Masterpact MTZ via NFC

Product String Reference:
  1. Top Level > Product Category > Buildings & IT > Partner Project Transactional > Air Circuit Breakers > ACB MTZ Communication
  2. Top Level > PR_Product_OPS_Structure > Circuit Breakers and Switches > High Current Air Circuit Breakers > Masterpact MTZ

Objective:
The objective of this video is to provide guidance of how to communicate with a Masterpact MTZ via NFC.




Product Line:
High Current Air Circuit Breakers

Environment:
N/A

Resolution:
  1. Download the Masterpact MTZ from the Play Store or App Store. Register if required. NFC will work both in circuit open and closed conditions. Micrologic X can communicate with internal battery and does not require power.
  2. Open the app and click NFC
  3. Hold it before the Micrologic X unit.
  4. When connected, it will be able to read the data from the Micrologic X
  5. Information provided include: Serial number, product reference, hardware and firmware reference.

Schneider Electric Global