{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Can all contact blocks be used for the 30mm range joysticks? [Video]

Question:
Can all contact blocks be used for the 30mm range joysticks?

Product String Reference:

  1. Top Level > Product Category > Industry > Industry Control & Drives > Control, Relays & Sign > Diameter 30.
  2. Top Level > PR_Product_OPS_Structure > Pushbuttons, Switches, Pilot Lights and Joysticks > 30mm Push Buttons > Harmony 30mm 9001K Metal Push Buttons

Objective:
The objective of this video is to provide an in-depth analysis of contact blocks and their application.



Product Line:
IDSIG - CONTROL, RELAYS & SIGN.

Environment:
N/A

Resolution:

When used in conjunction with a Harmony range push button, the:
  1. Combination N/O + N/C, N/C opens and N/O closes
  2. N/C contact opens when push button is depressed
  3. N/O contact closes when push button is depressed

When used in conjunction with the 30mm range joystick application.
  1. Combination N/O + N/C will stay open so that it is neither open nor closed
  2. N/C contact is open
  3. N/O contact is open
When the joystick is maneuvered, the:
  1. Combination N/O + N/C will close at different positions of the joystick handle.
  2. N/C will close
  3. N/O will close

As such, these contacts do not act in the same way for a joystick as they do for the Harmony range push button application.

Schneider Electric Global

Explore more
Range:
Harmony XK
Explore more
Range:
Harmony XK
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.