{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Will TwidoSuite software run on a Windows 10 machine?
Issue:
Can TwidoSuite run on Windows 10 ?

Product Line:
Twido, TwidoSuite

Environment:
TwidoSuite

Cause:
Can't get Twidosuite to run on Windows 10.

Resolution:
No. TwidoSuite, Twido is an obsolete product and has been replaced with the M221 and EcoStruxure Machine Exert Basic ( formally TwidoSuite) software that will run on Windows 10. The last version of TwidoSuite is version 2.31.4 and it will run on Windows 7 64 bit. With the Ecostruxure Machine Expert Basic and M221 you can import the old Twido programs into Machine Expert Basic and load program into the M221.

Schneider Electric Global