{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Compatibility of PM5100/PM5300 meter hardware with firmware versions

Product Line
PM5100
PM5300

Environment
Firmware

Resolution
  • Firmware revision 2.xx is applicable for PM51/53xx meters with enhanced internal memory.
  • Firmware V2.xx revision is applicable for Hardware version B1. Hardware version is indicated on the Meter labels
  • Firmware version 2.xx is not compatible with firmware version 1.xx.
  • Meters with 1.xx firmware can’t be upgraded with 2.xx firmware.
Refer to the attached What's New with V02.1x & V02.2x

Schneider Electric Global

Attachment(s)

PM51_53xx_Whats_New _V2.1x_V2.2x.pdfPM51_53xx_Whats_New _V2.1x_V2.2x.pdf [89.85 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: