The Compact NSX bare cable connectors (reference numbers listed in the attachment) can be used with solid or stranded cables.
Stranded cables, with cross sections indicated in the connectors instruction sheet, may be used without cable ends (ferrules). In case cable ends (ferrules) are used, it is advised to consider the maximum cross section compatible one size smaller than indicated in the instruction sheet. The cable end is increasing the diameter of the cable inserted in the connector.
Stranded cables, with cross sections indicated in the connectors instruction sheet, may be used without cable ends (ferrules). In case cable ends (ferrules) are used, it is advised to consider the maximum cross section compatible one size smaller than indicated in the instruction sheet. The cable end is increasing the diameter of the cable inserted in the connector.