{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the content of PCSPEAV98949 spare fuses for Accusine Active Harmonic Filters?
The content is:

Fuse Description                 Rating         QTY per Kit            Active Filter Size            Replaces Fuse
UL Type CC Slow Blow        6A 600VAC       1                          60A, 120A                         F1
UL Type CC Slow Blow        9A 600VAC       1                         200A, 300A                        F1
UL Type CC Slow Blow        4A 600VAC       3                             All                              F2, F3, F4
UL“ Solar” Fuse                  12A 1000VDC    3                             All                              F5, F6, F7

All 4-9Amp fuses are CC ferrule 10.3x38.1, type KLDR x  or FNQ-R-x (x..Amps)
12A fuse 0090.0012 (Schurter) or 0SPF012.T (Litelfuse)