What is the acceptable tolerance for the strip length of a cable to be connected to the EverLink cable connectors of the Compact NSXm?
For a correct installation of the wires to the EverLink cable connectors of Compact NSXm, the cables must be stripped to the length indicated in the supplied instruction sheet, with the accepted tolerance of -0mm / +2mm.
Released for:Schneider Electric Global
Explore more
Range:
ComPact NSXm
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.