The PowerPact series circuit breaker as shown in Schneider Electric Digest 178 Section 9 is not suitable to fit, and is not rated to be used with the NH1B panelboard. The NH1B panelboard does not have available short circuit ratings when used with the PowerPact series circuit breakers.
Released for:Schneider Electric Global