{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How does the GAVD0110 auxiliary contact work?
Issue:
Function of a GAVD0110 auxiliary contact.

Product line:
Tesys GV manual starters

Environment:
Auxiliary contacts

Cause:
Contacts do not appear to be working properly.

Resolution:
The GVAD** can only be installed on left side of product and the GV2 must be in OFF position when mounting.

The GVAD0110 has 2 different contacts
One is fault signaling contact (terminals 95/96) NC contact and the second is only standard auxiliary NO contact (terminals 53/54 ).

Fault signaling defect contact should be always in close position excepted when there is fault on GV2 ( short circuit or overload ) at this time contact open.
This fault signaling defect contact is not related to ON/OFF position of GV2’s but to reset back to NC the device must be switched back to the ON position.

Auxiliary contact report the ON/OFF position of GV2’s.
This Auxiliary NO contact is on Open when GV2 is on OFF position and close when GV2 is ON position.

Schneider Electric Global