{}

Welcome to the Schneider Electric corporate Website

Search FAQs
How can you set, change or remove the password on the Process drives using the Somove software?
Issue:
Customer wants to reset the password using Somove software.

Product Line:
Somove and Process Drive ATV630 and ATV930.

Environment:
All

Cause:
Reset the password using Somove.

Resolution:

On SoMove, going: Device -> Protection, you have the same features when using keypad`s: Main menu -> 4.Password .
Level1/Level2 corresponds to: PIN1/PIN2.

1. To set the password:





2. To change the password:





3. To remove password:



4. Protecting the SoMove file can be done by File/Project properties:







Schneider Electric Global

How can you set, change or remove the password on the Process drives using the Somove software?
Issue:
Customer wants to reset the password using Somove software.

Product Line:
Somove and Process Drive ATV630 and ATV930.

Environment:
All 

Cause:
Reset the password using Somove.

Resolution:

On SoMove, going: Device -> Protection, you have the same features when using keypad`s: Main menu -> 4.Password .
Level1/Level2 corresponds to: PIN1/PIN2.

1. To set the password:





2. To change the password:





3. To remove password:



4. Protecting the SoMove file can be done by File/Project properties:







 

Schneider Electric Global

Explore more
Product:
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Explore more
Product:
move-arrow-top