{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the main features of EM6438H meter ?
The EM6438H meter supports many features, a few of the features are listed below:

• LED display screen: Intuitive self-guided navigation using four buttons LED display, with three lines of concurrent values, and load bar that indicates current loading
• Energy accounting and balancing
• Alternate source, and RS-485
• THD% for voltage and current, per-phase • Active, reactive, and apparent energy readings
• Cyber security: The meter enables disabling the RS-485 port through front panel keys against unauthorized access. This feature can also be used for toggling         between the RTU devices in case of limited availability of nodes in software system
• Measurement of True PF

Schneider Electric Global