{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
PM8000 series firmware version 2.2.1 and release notes
Issue
PM8000 series firmware version 2.2.1 and release notes

Product Line
PM8000 series meter

Environment
PM8000 series firmware

Cause
A user would like to upgrade the firmware on a PM8000 series meter to V002.002.001

Resolution
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.*

*Warning: Devices should be disconnected from all monitoring software before performing a firmware upgrade*


NOTE: To apply this firmware, the meter must have firmware v2.1.0.

Release Notes: PM8000 firmware to address new and updated features for firmware version 2.2.1

For PM8000 V002.002.001 Firmware and Associated Files: 'PM8000 v 2.2.1 firmware'

Notes: This firmware update is intended for PowerLogic PM8000 meters. ION Setup 3.2 or later must be used.

Please downloaded ION Setup 3.2 before upgrading the PM8000 to firmware v2.2.1 'ION Setup Latest Release'

For instructions on upgrading the firmware using ION Setup, please follow knowledge base article FA244316

Schneider Electric Global