Search FAQs
What can cause an INF4 fault on the ATV61 and ATV71 drives?
Issue:
INF4 fault on the ATV61 and ATV71.
Product Line:
ATV61 and ATV71 drives
Environment:
All
Cause:
INF4 is an Internal Zone Fabrication Error which is caused by incoherent internal data on the EEPROM.
Resolution:
* Recalibrating the drive using the diagnostic menu. (This option is only available for the field services techs)
* Change the control bloc or power board.
INF4 fault on the ATV61 and ATV71.
Product Line:
ATV61 and ATV71 drives
Environment:
All
Cause:
INF4 is an Internal Zone Fabrication Error which is caused by incoherent internal data on the EEPROM.
Resolution:
* Recalibrating the drive using the diagnostic menu. (This option is only available for the field services techs)
* Change the control bloc or power board.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: