Search FAQs
Does the PM5560 support a simultaneous EtherNet/IP and Modbus TCP connection?
Issue
The customer asks if the PM5500 series meter can support a simultaneous EtherNet/IP and Modbus TCP connection.
Product Line
PM5560 (METSEPM5560)
PM5563 (METSEPM5563)
Environment
Communication Protocols
Resolution
Yes, the PM5560 series meter can handle a simultaneous EtherNet/IP and Modbus TCP connection.
Note: The PM5500 supports EtherNet/IP as of firmware version 2.5.2.
The customer asks if the PM5500 series meter can support a simultaneous EtherNet/IP and Modbus TCP connection.
Product Line
PM5560 (METSEPM5560)
PM5563 (METSEPM5563)
Environment
Communication Protocols
Resolution
Yes, the PM5560 series meter can handle a simultaneous EtherNet/IP and Modbus TCP connection.
Note: The PM5500 supports EtherNet/IP as of firmware version 2.5.2.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: