{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What can cause an InFN or error 23 fault on the ATV630 or ATV930 Process drives?
Issue:
InFN or error 23 fault on the Process drives.

Product Line:
ATV 630, 930 680 980 etc

Environment:
All

Cause:
A communication interruption between the control block and the AFE or the BU bricks has been detected.

Resolution:
- First check to see if they have wired their ethernet cable into the drives modbus ports.  This normally cause the main display to go blank and control block goes offline.
- Check the internal wiring between the control module line board and the AFE and or BUO's
- Check the LED801 on the control board of the AFE brick) red means communication interruption.
- Change the module link board.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: