Issue:
Configure Windows to use PowerChute Business Edition v10 SNMP in conjunction with Windows SNMP and SNMP Trap Services.
Product Line:
PowerChute Business Edition versions 10.0 and above
NOTE: PowerChute Business Edition versions 9.2.1 and below use the Windows SNMP service; see Configuring the Windows SNMP Agent for use with PowerChute Business Edition versions 9.2.1 and below for more details.
Environment:
All supported Windows operating systems
Cause:
Informational
Solution:
Windows SNMP Setup
- Open “Programs and Features” by clicking the Start button, selecting “Windows System” > “Control Panel,” and then clicking “Programs and Features.” From “Programs and Features,” select “Turn Windows Features On or Off.”:
Alternatively, you can directly access the Windows Features dialog box by clicking the Start button and typing “Turn Windows Features On or Off.”Scroll down and enable “Simple Network Management Protocol (SNMP)”:
PowerChute Setup
- Install PowerChute if necessary.
- Enable SNMP v1 and/or v3 from the SNMP Settings screen if necessary.
- In the “Miscellaneous” section, update the Discovery Port from 161 to a free port, e.g., 163 (161 and 162 are the well-known SNMP ports). You will see the error below if you do not make this change. Click Apply to save your changes.
Remove the conflicting Registry entry
- Click on the Start button, type regedit to launch the system registry editor, and delete the following registry Key:
- Open Control Panel - Administrative Tools - Services and restart the PowerChute Windows Service
- Restart the Windows Services
- Create a new PowerChute Agent IP/Port (Port from Step 5) mapping entry in your NMS.
- Test your changes.
Released for:Schneider Electric Global
Issue:
Configure Windows to use PowerChute Business Edition v10 SNMP in conjunction with Windows SNMP and SNMP Trap Services.
Product Line:
PowerChute Business Edition versions 10.0 and above
NOTE: PowerChute Business Edition versions 9.2.1 and below use the Windows SNMP service; see Configuring the Windows SNMP Agent for use with PowerChute Business Edition versions 9.2.1 and below for more details.
Environment:
All supported Windows operating systems
Cause:
Informational
Solution:
Windows SNMP Setup
- Open “Programs and Features” by clicking the Start button, selecting “Windows System” > “Control Panel,” and then clicking “Programs and Features.” From “Programs and Features,” select “Turn Windows Features On or Off.”:
Alternatively, you can directly access the Windows Features dialog box by clicking the Start button and typing “Turn Windows Features On or Off.”Scroll down and enable “Simple Network Management Protocol (SNMP)”:
PowerChute Setup
- Install PowerChute if necessary.
- Enable SNMP v1 and/or v3 from the SNMP Settings screen if necessary.
- In the “Miscellaneous” section, update the Discovery Port from 161 to a free port, e.g., 163 (161 and 162 are the well-known SNMP ports). You will see the error below if you do not make this change. Click Apply to save your changes.
Remove the conflicting Registry entry
- Click on the Start button, type regedit to launch the system registry editor, and delete the following registry Key:
- Open Control Panel - Administrative Tools - Services and restart the PowerChute Windows Service
- Restart the Windows Services
- Create a new PowerChute Agent IP/Port (Port from Step 5) mapping entry in your NMS.
- Test your changes.
Released for:Schneider Electric Global