{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is possible to read 32 bit variable with OFS when using the .csv option?
Issue
How to read a variable of 32 bit on OFS when using .csv option?

Product Line
OPC Factory Server (OFS), Ecostruxure Control Expert, M580

Environment
OFS v3.62, Control Expert v14.1, Windows 10 version 1902 (OS Build 18362.30), BMEP586040 v2.90, CitectSCADA 2018 R2

Resolution
The OFS has an option to use a .csv as symbol table file when the server is communicating with a device by Modbus and the OFS documentation shows the example as a register that is a INT variable, but you can also declare DINT variable on the .csv file as shown below:
  • Device address for the csv file on OFS configuration tool
MBT:IP_Address/NQ
  • format of the line on the csv file
%MDx,Symbol,Comment

When you declare the variable with this syntax, the CitectSCADA will import the variable as LONG with 32 bits.

img1

Schneider Electric Global