{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Are the 9001 KA contact blocks gold flashed?
Issue:
Do we have contact blocks with gold flashed terminals for 30mm push buttons?

Product Line:
Push Buttons and Operator Interface

Environment:
30 mm Push buttons and accessories

Resolution:
Not on the standard contact blocks. We have a 9001KA3* series that has gold flashed contacts.

1NO and 1NC - 9001KA31
1NO - 9001KA32 (OBSOLETE)
1NC - 9001KA33
1NO Early Closing - 9001KA34
1NO Late Opening - 9001KA35

Schneider Electric Global