{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
BMXCRA312x0 and the BMECRA312x0 remote adapters 'Custom RPI' parameters settings does not work.
Custom RPI settings for the BMXCRA312x0 or BMECRA312x0 remote adapters do not work when using Unity V13.1, CE V14.0, or CE V14.1.

For example, if the RPI is set to 31ms in the following configuration,


The RPI does not display the change in the DTM.


The issue is resolved in:
  • Control Expert V15.0
  • Control Expert V14.1 using HotFix1 (HF1)

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: