undefined undefined
{}

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the effects of dV/dt on a Motor when using a VSD?
As there is an impedance mismatch at the termination of the motor cable to the motor, there will be a reflected wave which travels back along the motor cable causing
overvoltage’s. Overvoltage’s on the motor terminals can cause both partial and corona discharge which eventually wears down the winding insulation to failure.

Corona discharge occurs when the overvoltage is large enough to cause electrons to flow from one winding to another whilst ionising the air between the conductors. They cause damage to the internal and external insulating material respectively. As the motor cable length increases the peak voltage increases. This can increase to a value of 2 to 2.5 times the DC bus voltage.

Schneider Electric Offer Sinus filters or dv/dt filters to reduce the overvoltage across windings and high frequency currents in differential mode. Check out our current ATV600 or ATV900 catalogue for more information on output filters to help you with overvoltage mitigation.

Schneider Electric Global

Explore more
Category:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.