{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Settings Required to Connect Gurux DLMS to ION meters

Issue
User unable to connect to ION meter via DLMS
_____________________________________________________________

Product Line
ION9000
ION8650
ION8800
ION7400
_____________________________________________________________

Environment
Gurux DLMS Director
_____________________________________________________________

Solution
Different software may require different settings. The settings below are for Gurux DLMS Director. Values are in hex. For example Physical server 64 is decimal 100.

Start Protocol: DLMS
Logical Name Reference: Checked
Authentication: None
Client address 10
Physical Server 64
Host Name: IP address of meter
Port: Port defined on the meter, default is 4059
Protocol: Tcp
Use Serial port through ethernet: Checked
_____________________________________________________________

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: