{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the syntax of the ADDM for READ_REMOTE EFB when using through BMENOC03x1 ?
If you are using the READ_REMOTE EFB to read the remote variables from another PLC and the Ethernet modules used to send the request is a BMENOC03x1, the syntax of the ADDM EFB depends on the firmware version of the BMENOC03x1 modules:
  • Firmware older than v2.19: 'r.m.c{IP_Address}TCP.MBS'
  • Firmware v2.19:  'r.m.c{IP_Address}'
As you can see below, you do not need to specify the TCP.MBS if you are using the BMENOC03x1 firmware v2.19 .
READ_REMOTE

Schneider Electric Global

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: