{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Masterpact MTZ: Components needed to locally operate breaker via smartphone app
Issue: Local operation via phone app capability was not ordered from the factory.  Need to field modify.
Product Line: Circuit Breakers
Environment: Masterpact MTZ

Resolution: to field modify, the following components are required. Some of these parts may already be installed.
  • Mobile App – EcoStruxure Power Device
  • Masterpact Operation Assistant Digital Module LV850005
  • XF-Com, MX-Com coils, part numbers vary based on voltage.
  • Spring Charging Motor, part numbers vary based on voltage.
  • Isolation Module LV850056SP
image.png
  • Isolation Module to coils communication cables MTZ1: LV833118SP, MTZ2/MTZ3: LV847904SP
image.png
  • MX-Com cable needs to be plugged into the MX1 location on Isolation module, not MX2.
image.png
  • Coils properly wired, C3 and A3 continuously powered. C2 and A2 are only needed for push button operation.
image.png
  • Accessories Declared in the Control Unit via EPC, click the accessory pencil
image.png


Then declare accessories
image.png

Schneider Electric Global