Search FAQs
Does the EcoStruxure OPC UA server Expert support extracted bits of a integer ?
Issue:
Support of extracted bits for Variables with Data Type INT or UINT
Product Line:
OPCUAServerExpert V2.01 SP1, M580
Resolution:
Yes. With Ecostruxure OPC UA Server Expert V2.01 SP1 it is possible to address an extracted bit of a Variable with Data Type INT or UINT. For instance, to address the extracted bit 4 of a Variable with NodeID "s=0:M580!MyVar", address the NodeID "s=0:M580!MyVar.4"
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: