{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to solve the error message of E2558 multiple networks in macro section?
  1. Issue

Customer has concerted one PL7 application into Control Expert where it pops up “E2558 multiple networks in macro section (solution for SFC-Project-Setting 'Allow multiple token': move this network to chart section)”
How to solve this error message?
  1. Environment
E2558, SFCcontrol expert
  1. Resolution

The message is self-explainable as inside macro section, there only allows one network.
The problematic part is illustrated in the blue rectangle

Diagram  Description automatically generated
The fix solution is illustrated below
Diagram, schematic  Description automatically generated



Schneider Electric Global