Search FAQs
What is the difference between TeSys Giga advanced and standard type contactors ?
The advanced type has 3 coil variants to cover 24V-500V control voltage, PLC control input, lower coil consumption, cable memory kit, feasibility to fix Remote wear Diagnosis (RWD) module.
Whereas the standard version comes with two coil variants to cover 48-250V control voltage, normal coil consumption and with direct coil control by A1/A2.
Both advanced and standard versions have self-diagnosis LED on the front of the contactor to indicate the main contact life, over and under voltage indication, internal fault indication etc..
Whereas the standard version comes with two coil variants to cover 48-250V control voltage, normal coil consumption and with direct coil control by A1/A2.
Both advanced and standard versions have self-diagnosis LED on the front of the contactor to indicate the main contact life, over and under voltage indication, internal fault indication etc..
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: