undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
GOOSE communications periodically drops out and comes back.
This can occur if the imported third party IED device CID file does not have the GOOSE 'MinTime' or 'MaxTime' field for the GOOSE subscribe delay timeout.

A fix has been implemented in exec firmware version 2.4 where it will set an appropriate default value when there's no 'MinTime' or 'MaxTime' field in 3rd party CID file.  The fix is described as a stability enhancement in the release notes.

To resolve the issue, update to the latest exec firmware.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: