Is EVlink Pro AC compliant with EV READY EV41 (Current floor value) ?
Article available in these languages:Czech
Yes. The Evlink Pro AC measures the reactive current. If the reactive current is higher than 2,5A phase by phase during 1 minute, the floor value will be 14A for 3-phase charging or 8A for single-phase charging.
Released for:Schneider Electric Global
Explore more
Range:
EVlink Pro AC
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.