{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Video: eConversion Live from the Lab 3: Power Factor Correction

eConversion is a patented high-efficiency mode for Schneider Electric Galaxy V Series (VS, VM, VL, VX) UPS that combines the best efficiency (up to 99%) with maximum load protection (IEC62040-3 class 1, VFI1.1.1 – equivalent to Double Conversion). eConversion typically provides a 3x reduction of the UPS electricity consumption.
This live video from the lab shows how eConversion performs input power factor correction.
Discover more via eConversion Savings Calculator.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: