{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to check which hardware and software of the M580 Safety Processor offer is TÜV certified for safety PLC programming?
1.Issue:
How to check which hardware and software of the M580 Safety Processor offer is TÜV certified for safety PLC programming?

2. Product Line:
M580 Safety Processor
Unity Pro
Control Expert L or XL
M580 Safety Add On
X80 modules
M580 communication modules

3.Enviroment
PLC Configuration Software in Windows and physical hardware

4.Cause
I need to know if the M580 Safety Processor hardware and software is TÜV certified for my application.

5. Resolution:
This article is valid for the X80 modules offer, M580 communication modules , M580 Safety Processor and the Control Expert L or XL with M580 Safety Add On software

TÜV certified Control Expert versions and hot fixes:

With certificate 01/205/5610.02/22 and the latest revision version 5.0.

For safety PLC programming the approved TÜV versions of Control Expert and released hot fixes (HF) are the following:
Control Expert L or XL with M580 Safety Add On list Part 1
Control Expert L or XL with M580 Safety Add On list Part 2

TÜV certified M580 Safety Processors, M580 communication modules and X80 modules:

In the revision list, you can also find the status of the different X80 modules, communication modules and M580 Safety Processors.

X80 modules
Part of the X80 modules list
Note: The above image is only one part of the list of X80 modules.

M580 communication modules
M580 communication modules
Note: The above image is only one part of the list of M580 communications modules.

M580 Safety Processors
M580 Safety Processors
----------

Check the TÜV certification status:

To check if a software version of Control Expert or Hot fix is TÜV certified or if it is certified to date, we must do the following:
  • Go to: https://www.certipedia.com/
  • In Search tool prompt “M580”, then select the newest certificate from the SCHNEIDER ELECTRIC certificate holder.
Select latest M580 certificate
  • Then click on the list located in Appendixes.
From the Certificate select Appendixes
  • And then search for the hardware part, software version or hot fix you need.

If the hardware, software version or hot fix is not in the list, it means it is not TÜV certified.

Schneider Electric Global

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: