{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Testing your Geo SCADA application after an upgrade
Below are some common areas to test after an upgrade to a newer version of Geo SCADA takes place:
  • The database server starts as expected, no errors occur during the start up
  • The server’s license is being recognized
  • The ViewX clients are licensed and connect to the database server as expected
  • All outstations are able to communicate to their respective devices
  • Data arrive as expected from the outstations
  • Mimic navigation works as expected
  • Mimic scripts are able to run without errors
  • For redundant systems:
    • All redundant servers are able to synchronize with the main server
    • Server changeover works as expected
  • For Virtual ViewX:
    • Virtual ViewX server is upgraded as well as the rest of Geo SCADA
    • Virtual ViewX clients are able to connect to the database server
  • 3rd party clients are able to connect to Geo SCADA and perform their tasks

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: