{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to reset the Geo SCADA super-user account in case you forgot the password
It is possible to reset the Geo SCADA super-user account in case its password is lost. The user must have Windows Administrative rights to that computer.
The procedure is the following:
  1. Shutdown the Geo SCADA Server, wait until it is down, with the Server icon in gray color
  2. Go to Windows Control Panel and select the “Programs and Features” option:
Programs
  1. Under “Uninstall or change a program”,  click on “Schneider Electric EcoStruxure Geo SCADA Expert 2020” (or the version you have installed) and select the “Change” option:
Change
  1. This will bring the Geo SCADA installation splash screen. Click on “Next”:
Splash
  1. Click on “Modify”:
Modify
  1. Check the “Change Super-User Account” check-box (don’t change anything else) and click on “Next”:
Checkbox
  1. Enter the super-user "User Name" and password, then click on “Next”:
user
  1. Click on “Install”:
install
  1. Click on “Finish”:
finish

  1. Now you can start Geo SCADA Server. The new account will be available for use. Note that the super-user account must be used carefully and should not be of public knowledge. Best practice is to disable it when an application has proper security settings in place.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: