{}

Welcome to the Schneider Electric corporate Website

Search FAQs
Checking Realflo Licenses with SCADAPack x70 RTU's
On previous generations of SCADAPack such as the SCADAPack 32, SCADAPack 3xx or SCADAPack 4203 series RTU's, Realflo licenses where specific to type and run number. For example a SCADAPack 4203 could have 2 gas runs OR 1 gas, 1 water and 1 liquid. These were determined by the actual license of the device.

On a SCADAPack x70 RTU, Realflo licenses are for number of runs. Type is decided by the user. Example a user could have 10 flow runs licensed. This could be for any type of runs. The user can decide via the Realflo configuration if it uses 2 gas runs, or 9 liquid run and 1 water run, or 5 gas runs with 5 liquids runs or even just 1 gas run. Essentially any combination of 10 runs or less.

To check to see how many runs a SCADAPack x70 device is licensed for for, the user can open either RemoteConnect or Realflo.

RemoteConnect
  • Create a default 47x or 57x project using RemoteConnect version 2.6.1 or later
  • Connect to the RTU via RemoteConnect and go online (via Modbus TCB/USB or DNP3 USB)
  • Check the "Online Diags - SPx70 Controller tab"
  • Refresh the page
  • The amount of flow runs that can be configured in Realflo is displayed
RCLic

Realflo
  • Open Realflo version 7.00 or greater in Expert mode
  • Select "File -> New" from the drop down menu
  • On the Create New pop-up, select "Create 1-run gas configuration with default values"
  • Select Configuration -> PC Communication Settings
  • Set proper PC Communication settings as per your set-up
  • Select Configuration -> Flow computer information from the drop down menu
  • The amount of flow runs available and that are configured is available

RFLic


For more information, please see the RemoteConnect and Realflo help files installed with each software respectively.
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
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.