{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How many devices can be connected to an HMIGTO by using SoMachine Protocol?
Some customers use an HMIGTO in their configuration and they would like to know the number of devices (M241, M251, etc..) they can connect to the HMI by using SoMachine Protocol/Machine Expert Protocol.
The goal of this article is to inform about the number of devices supported by an HMIGTO by using SoMachine Protocol/Machine Expert Protocol.

This article is applicable to the following products:
HMIGTO

This topic is related to Vijeo Designer

The current version of Vijeo Designer (VJD 6.2 SP12) allows only 4 connections for an HMIGTO when using SoMachine Protocol/Machine Expert Protocol.
If you have more than 4 devices to connect to an HMIGTO, please consider using Modbus Protocol for some devices.

Schneider Electric Global

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: