Search FAQs
Deployment of Data Center Expert 7.9.x VM only allows up to 8 CPU cores.
Issue:
Deployment of Data Center Expert 7.9.x only allows up to 8 CPU cores.
Product Line:
Data Center Expert
Environment:
DCE potentially any version
AP94VMACT deployment on VMware ESXI
Cause:
Data Center Expert VM was only built with the maximum capacity of 8 CPU cores. This was due to compatibility with ESXI version 4.
Resolution:
This can be edited in VMware and changed to allow more cores.
Shut the vm down.
Right click the VM in vsphere.
Go to Compatibility --> Upgrade Compatibility
![conmpatibility_menu.PNG](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DBqEPQA1&oid=00DA0000000abSmMAI)
You will get a warning stating that this is an irreversible operation. Hit yes.
![compatibility_warning.PNG](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DBqEQQA1&oid=00DA0000000abSmMAI)
Choose the last one in the "Compatible With" list and hit OK
![compatible_with.PNG](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DBqERQA1&oid=00DA0000000abSmMAI)
You should now be able to set over 8 CPUs for the DCE 7.9.2
![compatible_edit_settings.PNG](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000DBqESQA1&oid=00DA0000000abSmMAI)
***Please note that if you have deployed a version and increased the number of cores, then upgraded that version to the next (not a fresh VM deployment), you will not see this issue.
Deployment of Data Center Expert 7.9.x only allows up to 8 CPU cores.
Product Line:
Data Center Expert
Environment:
DCE potentially any version
AP94VMACT deployment on VMware ESXI
Cause:
Data Center Expert VM was only built with the maximum capacity of 8 CPU cores. This was due to compatibility with ESXI version 4.
Resolution:
This can be edited in VMware and changed to allow more cores.
Shut the vm down.
Right click the VM in vsphere.
Go to Compatibility --> Upgrade Compatibility
You will get a warning stating that this is an irreversible operation. Hit yes.
Choose the last one in the "Compatible With" list and hit OK
You should now be able to set over 8 CPUs for the DCE 7.9.2
***Please note that if you have deployed a version and increased the number of cores, then upgraded that version to the next (not a fresh VM deployment), you will not see this issue.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: