{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

How can you set up the EADM software to update an ATV340, ATV630 or ATV930 Drives firmware?

Issue:

EADM or EcoStruxure Automation Device Maintenance software to update an ATV340E, ATV630 or ATV930 Drives firmware?

Product Line:

ATV340E, ATV630 and ATV930

Environment:

All

Cause:

Firmware update tool

Resolution:

Step 1

Download theEcoStruxure Automation Device Maintenance or EADM software package version 3.1 or higher.

a

Step 2

Two certificates must also be installed.

https://download.schneider-electric.com/files?p_Doc_Ref=PKICER_ROOTCA

https://download.schneider-electric.com/files?p_Doc_Ref=PKICER_TIMESTAMPCA

Step 3 After you have downloaded the EADM software and certificates to your PC open and run the EADM software and the certificates.

Step 4 Temporary disable your anti-virus firewall. Otherwise, you cannot connect your PC to the Drive using Ethernet.

b

Step 5 Now open the EADM Software and connect a CAT 5 Ethernet cable to your PC and to the Drives Ethernet port.

Step 6 Setup your PCs Ethernet port with an IP and subnet address under the Ethernet Settings in your PC. Example Choose IPV4 setup and set the address to 192.168.1.2 and subnet address to 255.255.255.0

c

Step 7 Setup your Drives IP example and subnet address using an VW3A1111 HM in the Communcations and Ethernet settings tab. You must power cycle the Drive after setting up the IP address.

Example settings

Comm Parameters menu then Ethernet:

Device Name: Test example

IP mode: Fixed

IP address: 192.168.1.10

Subnet address: 255.255.255.0

Power cycle the Drive at this point.

Step 8 Open up the EADM software and go into the settings menu.

-Discovery TAB- Make sure that the DPWS and Modbus TCP are both enabled.

d

Step 9:

Settings menu

Modbus TCP- setup your Drives IP address to find. In this example it will be the Drives IP address 192.168.1.10

e

Step 10:

Settings

Choose: Package Settings: Select the path to the Drives firmware packages.

f

Step 11:

The Drives firmware packages should now be visible under the "Data Packages" Tab.

g

Step 12:

Under the Device Loading TAB click on the Device discovery icon to search and find the drives IP address.

h

Step 13:

Verify that it found the Drive that you searched for. Then click on Set credentials if your Drive has cyber security you will need to enter the username and password to connect.

i

j

If cyber security is disabled, you can choose and select Anonymous and connect.

k

Step 14

Now you can select the Firmware version you want.

Click on the Update Center icon and select Firmware.

l

Step 15

Choose the Frame size firmware to be updated into the Drive

Example Frame size 1 wall mount is S1- 6 is selected or it will show the ATV6XX U07- C16

m

Step 16:

Select the drive that needs the firmware updated.

n

Step 17: Now choose or click on the Update button at the bottom of the page.

o

Step 18:

If you are in a safe condition, you can choose optional box at the bottom and the firmware update begins.

p

Step 19 confirm Software update was complete.

u

Done.

Schneider Electric Global

Explore more
Range:
Altivar Process ATV600Altivar Process ATV900Altivar Machine ATV340
Explore more
Range:
Altivar Process ATV600Altivar Process ATV900Altivar Machine ATV340
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.