{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

How to update firmware on SCADAPack 6000 series I/O modules

When using a SCADAPack x70 device (57x, 47x, 47xi), 6000 series expansion I/O modules can be added to the SCADAPack for additional input/outputs. These differ from the legacy 5000 series modules where firmware can be updated on the 6000 series if needed. RemoteConnect can be used to update the I/O modules.

By default, when RemoteConnect is installed, the firmware file is stored in the following directory, where x.xx.xx represents the current version:
64-bit systems: C:\Program Files (x86)\Schneider Electric\RemoteConnect\Firmware\660x\x.xx.xx

Use SCADAPack RemoteConnect to transfer the .bin firmware file to the SCADAPack file system:
  • Connect SCADAPack RemoteConnect to the SCADAPack x70 device and go Online.
  • Under My Network, right-click on SCADAPack x70 Controller Settings -DeviceDTM and select Additional Functions > Write File to Device.
  • In the Write File to Device dialog, click Browse to navigate to the location of the file on your computer.
  • Click Open.
  • In the Write File to Device dialog, click OK.
  • Under My Network, right-click on SCADAPack x70 Controller Settings -DeviceDTM and select Additional Functions > Execute Command.
  • Enter the command:
restart iofirm fw6607_Version.bin module_address
Where the module_address is the address of your I/O module. The I/O module address is a number from 0 to 15. The 6607 module located inside a SCADAPack 474 is always address 0.
Example: restart iofirm fw6607_Version.bin 0

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: